PN7150 Output power?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 Output power?

1,975件の閲覧回数
erkka_laine
Contributor I

Hi, I'm looking for PN7150 output power for the type approvals. I can't find this information of the datasheet.

ラベル(1)
0 件の賞賛
返信
1 返信

1,782件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes, there is  not the type value for it. One may refer to the below information.

The PN7150 has also a programmable transmitter output power from 3.0V to 4.75V even if not given in dBm.

 PN7150 can have TVDD adjustable and depending on the Impedance Tuning also the Current consumption is different.

Example: if a Tuning at 20ohm is done the IC can drive approx 1Watt of Output power to the Antenna (TVDD = 5V and ITVDD = 0.2A).

Hava a nice day.

Best regards

0 件の賞賛
返信