PN7150 Factory Test App

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 Factory Test App

2,498件の閲覧回数
sivasu4098
Contributor III

Hi all,

I am using PN7150 chip to test the MIFARE cards in custom board . Using the following test app to read the card information.

nxpnfc_android_nougat/FactoryTestApp at master · NXPNFCLinux/nxpnfc_android_nougat · GitHub 

Whenever  running the application , getting the following response. Please help me to proceed  further for testing of cards.

./data/NfcFactoryTestApp                                           

----------------------------
NFC Factory Test Application
----------------------------
PN7150 NFC controller detected
Select the test to run:
     1. Continuous RF ON
     2. PRBS
Your choice: 1
Continuous RF ON test
NFC Controller is now in continuous RF ON mode - Press enter to stop

Thanks and Regards,

Sivasubramaniyan

0 件の賞賛
返信
1 返信

2,321件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For the details of using Factory Test Application, please refer to Chapter 5 of https://www.nxp.com/docs/en/application-note/AN11690.pdf

0 件の賞賛
返信