PN7150 Andriod 10 VTS Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 Andriod 10 VTS Issue

5,251 Views
bob_zhang
Contributor I

Customer use PN7150 on Android 10. Application layer cann't find PN7150 device when do VTS test using Google original system.img. There is no migration guide of Android 10 in AN11690 file.The log file show as attached file. Please help analyse.Thanks!

Labels (1)
0 Kudos
Reply
3 Replies

5,234 Views
jimmychan
NXP TechSupport
NXP TechSupport

Hi,

 

According to your log file, the I2C write is failed. Please double check the I2C setting (e.g. I2C setup in device tree file).

 

For your reference : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/PN7150-NFC-Controller-on-i-MX8M-mini-evk...

 

 

0 Kudos
Reply

5,229 Views
bob_zhang
Contributor I

Hi Jimmy,

   Customer checked the I2C setup,and make sure I2C work properly now. There are new failure show as attached file. Please help check. 

0 Kudos
Reply

5,219 Views
jimmychan
NXP TechSupport
NXP TechSupport

Did customer follow the document porting the Android Q?

https://www.nxp.com/docs/en/application-note/AN11690.pdf (Section 3.1)

Also, please run the Factory Test (Chapter 5) and check the Chapter 6 "Troubleshooting".

0 Kudos
Reply