ntp5312 read tag uid

cancel
Showing results for 
Search instead for 
Did you mean: 

ntp5312 read tag uid

161 Views
VAZN
Contributor I

Hello everyone, 

I want to use the NTP5312 to read/write nfc tags. 

I have read the data-sheet but I don't find the way to do it. Should I use the SRAM and i2c to NFC pass-through to read and write nfc tags?

Thank you very much for your help

 

 

0 Kudos
1 Reply

149 Views
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. Do you want to read/write on the NTAG5 or do you want to read/write other NFC tags with the NTP5312?

 

The NTAG 5 link is a NFC Tag, so you cannot use it to interact with other tags, you must have a NFC Reader to interact with the tags.

 

You can see our Recommended NFC Readers in this page: NFC Readers.

 

Best Regards,

Ricardo

0 Kudos