PN7150 Andriod 10 VTS Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 Andriod 10 VTS Issue

5,249件の閲覧回数
bob_zhang
Contributor I

Customer use PN7150 on Android 10. Application layer cann't find PN7150 device when do VTS test using Google original system.img. There is no migration guide of Android 10 in AN11690 file.The log file show as attached file. Please help analyse.Thanks!

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

5,232件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Hi,

 

According to your log file, the I2C write is failed. Please double check the I2C setting (e.g. I2C setup in device tree file).

 

For your reference : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/PN7150-NFC-Controller-on-i-MX8M-mini-evk...

 

 

0 件の賞賛
返信

5,227件の閲覧回数
bob_zhang
Contributor I

Hi Jimmy,

   Customer checked the I2C setup,and make sure I2C work properly now. There are new failure show as attached file. Please help check. 

0 件の賞賛
返信

5,217件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Did customer follow the document porting the Android Q?

https://www.nxp.com/docs/en/application-note/AN11690.pdf (Section 3.1)

Also, please run the Factory Test (Chapter 5) and check the Chapter 6 "Troubleshooting".

0 件の賞賛
返信