PN7150 Activation Failure Notification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PN7150 Activation Failure Notification

跳至解决方案
2,579 次查看
wilmer_suarez
Contributor III

Hello,

While the PN7150 is scanning, it periodically attempts to activate a target and fails since no target triggered the activation. It is not negatively affecting the system I'm building, I'm just wondering what the reason might be that it keeps triggering an activation attempt when nothing to activate exists?

Thanks

标记 (3)
0 项奖励
回复
1 解答
2,497 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Thank you, I asked because this is not a known problem on the eval board with NXP's host MCU.

In this case please check your hardware, porting of the library, and possibly the environment where your project is at. It is recommended to first start with the eval board and host MCU for which the library was made and then move to a custom solution.

BR,

Ivan.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,497 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

May I ask if you are working with the evaluation board or a custom board and which host MCU?

Thank you.

BR,

Ivan.

0 项奖励
回复
2,497 次查看
wilmer_suarez
Contributor III

it is on a custom board. With an STM32f207

0 项奖励
回复
2,498 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Thank you, I asked because this is not a known problem on the eval board with NXP's host MCU.

In this case please check your hardware, porting of the library, and possibly the environment where your project is at. It is recommended to first start with the eval board and host MCU for which the library was made and then move to a custom solution.

BR,

Ivan.

0 项奖励
回复