NFC antenna question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC antenna question

1,635件の閲覧回数
bob_zhang
Contributor I

Our customer use PN7150. I test the antenna coil parameters. The Rcoil is 16.3ohm,is it a normal value?  Besides, the antenna coil locate on the battery, I see the L value change from 1.33uH(remove battery) to 1.2uH(with battery),what kind of influence lead to for the performance and what should we do?

ラベル(2)
0 件の賞賛
返信
1 返信

1,560件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

The antenna resistance value is not bad, normally a small value translates into more power to the antenna but taking care not to exceed max transmission current, whilst a bigger antenna impedance is recommended for battery-powered devices; please take a look to the antenna design app note for more information about this.

Regarding the antenna onto the battery, it would be helpful to have a material to isolate them, some recommendations are available in the antenna design videos for NFC.

Hope it helps you to comprehend.

BR,

Ivan.

0 件の賞賛
返信