PN7150 About Tag read error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 About Tag read error

7,072件の閲覧回数
h-kawada
Contributor II

I am troubled with the following operation of PN7150.

[ Execution environment ]

  BOARDs :
  1). OM5578/PN7150ARD
  2). LPCxpresso824-MAX

  IDE : MCUXpressoIDE 10.3.1
  Project : NXP-NCI_LPC82X_example
  NxpNci.c : '18/12/19 14:11
  nfc_task.c : '18/12/19 14:11

  PN7150 CORE_INIT_RSP :
  NCI << 40 01 19 00 03 1e 03 00 08 00 01 02 03 80 81 82 83 02 d0 02 ff 02 00 04 88 10 01 a0

  VICCs : ISO15693 NXP ICODE SLIX
  1) UID = e0 04 01 50 65 6d 40 b5
  2) UID = e0 04 01 50 65 6c 74 0f
  3) UID = e0 04 01 50 65 6c e9 df

[ Operation verification ]

  [1] 1 VICC : No.1
      NCI << 61 05 15 01 01 06 06 ff 01 0a 00 00 b5 40 6d 65 50 01 04 e0 06 80 80 00
       | RF_INTF_ACTIVATED_NTF <-- OK


  [2] 1 VICC : No.2
      NCI << 61 05 15 01 01 06 06 ff 01 0a 00 00 0f 74 6c 65 50 01 04 e0 06 80 80 00
       | RF_INTF_ACTIVATED_NTF <-- OK


  [3] 1 VICC : No.3
      NCI << 61 05 15 01 01 06 06 ff 01 0a 00 00 df e9 6c 65 50 01 04 e0 06 80 80 00
       | RF_INTF_ACTIVATED_NTF <-- OK

  [4] 2 VICCs : No.1 & 2
      NCI << 61 03 0f 01 06 06 0a 00 00 b5 40 6d 65 50 01 04 e0 02
      NCI << 61 03 0f 02 06 06 0a 00 00 0f 74 6c 65 50 01 04 e0 01
       | RF_DISCOVER_NTF <-- OK

  [5] 2 VICCs : No.1 & 3
      NCI << 61 03 0f 01 06 06 0a 00 00 b5 40 6d 65 50 01 04 e0 02
      NCI << 61 03 0f 02 06 06 0a 00 00 df e9 6c 65 50 01 04 e0 01
       | RF_DISCOVER_NTF <-- OK


  [6] 2 VICCs : No.2 & 3
      NCI << 60 07 01 a1
      NCI << 60 07 01 a1
       :
       :
      NCI << 60 07 01 a1
      NCI << 60 07 01 a1
       | CORE_GENERIC_ERROR_NTF <-- NG

       | A1 : DISCOVERY_TARGET_ACTIVATION_FAILED

[1] - [5] Normal operation.
[6] Why can't the PN7150 identify tags?

11 返答(返信)

6,549件の閲覧回数
h-kawada
Contributor II

PN7150B0HN/C11006 is installed
OM5578/PN7150ARD is
How can I get it?

The board I have now
I wish I could upgrade

0 件の賞賛
返信

6,549件の閲覧回数
h-kawada
Contributor II

Data Sheet

Modified Date : 25 Jun 2020

User Guide

Modified Date : 26 Jun 2020

Adder definition of PN7150B0HN/C11006

0 件の賞賛
返信

6,549件の閲覧回数
h-kawada
Contributor II

Hello

Thank you for your response

> We are planning to release a new version fixing

Waiting for good news

6,549件の閲覧回数
h-kawada
Contributor II
0 件の賞賛
返信

6,549件の閲覧回数
h-kawada
Contributor II

Discontinuation Notification 202001024DN

Why was PN7150B0HN / C11004E discontinued?

0 件の賞賛
返信

6,549件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Yes, I just received internal feedback about this. They let me know that we had to discontinue this version because of a major regression lately found.

We are planning to release a new version fixing this but are still waiting for R&D planning for which we will appreciate your comprehension on this.

Thank you very much.

BR,

Ivan.

0 件の賞賛
返信

6,550件の閲覧回数
h-kawada
Contributor II

Should have seen the latest datasheet sooner.


[ PN7150 Version ]

  NCI >> 20 01 00
  NCI << 40 01 19 00 03 1e 03 00 08 00 01 02 03 80 81 82 83 02 d0 02 ff 02 00 04 88 10 01 a0

  answer[8] : 0x08
  answer[17+answer[8]] : 0x10
  answer[18+answer[8]] : 0x01
  answer[19+answer[8]] : 0xA0

  Version C11002


[ PN7150 Product data sheet ]

  Rev. 3.9__28 August 2019
  317439

6 Versions

   6.1 Version C11004

      A fix has been added that addresses a collision
      resolution problem for ISO 15693 tags in case
      there are multiple tags in the field.

   6.2 Version C11002

      initial released version.


Equipped with PN7150B0HN / C11004
Does OM5578 / PN7150ARD exist?

0 件の賞賛
返信

6,549件の閲覧回数
h-kawada
Contributor II

Performed additional testing

  VICCs : ISO15693 NXP ICODE SLIX
  1) UID = e0 04 01 50 d6 bb 63 76
  2) UID = e0 04 01 50 d6 bb 63 09

[ Operation verification ]

  [1] 1 VICC : No.1

      NCI << 61 05 15 01 01 06 06 ff 01 0a 00 00 76 63 bb d6 50 01 04 e0 06 80 80 00
       | RF_INTF_ACTIVATED_NTF <-- OK

  [2] 1 VICC : No.2
      NCI << 61 05 15 01 01 06 06 ff 01 0a 00 00 09 63 bb d6 50 01 04 e0 06 80 80 00
       | RF_INTF_ACTIVATED_NTF <-- OK

  [3] 2 VICCs : No.1 & 2
      NCI << 61 03 0f 01 06 06 0a 00 00 76 63 bb d6 50 01 04 e0 02
      NCI << 61 03 0f 02 06 06 0a 00 00 09 63 bb d6 50 01 04 e0 01
       | RF_DISCOVER_NTF <-- OK

0 件の賞賛
返信

6,549件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please let me know if I understood your requirement.

When you try to read ICODE SLIX 1 & 2 specifically it is not possible to activate them? If so, have you modified something in the SW to detect multiple devices?

Thank you for clarifying.

BR,

Ivan.

0 件の賞賛
返信

6,549件の閲覧回数
h-kawada
Contributor II

Hello

Thank you for your reply


Yet I have not changed the settings
The same execution environment

[Anti-collision failure]

  UID = e0 04 01 50 65 6c 74 0f
  UID = e0 04 01 50 65 6c e9 df

[Anti-collision success]

  UID = e0 04 01 50 d6 bb 63 76
  UID = e0 04 01 50 d6 bb 63 09


After this, I want to change the PF_BIT_RATE setting.
Are there any other measures?

0 件の賞賛
返信

6,549件の閲覧回数
h-kawada
Contributor II

> After this, I want to change the PF_BIT_RATE setting.

Changing PF_BIT_RATE did not change the result

  Tried value :
    0x00 : 106k
    0x01 : 212k
    0x02 : 424k
    0x03 : 848k
    0x80 : 26k
    0x81 : 212k & 424k

0 件の賞賛
返信