PN532 Antenna Design question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PN532 Antenna Design question

跳至解决方案
11,258 次查看
shayohayon
Contributor II

Dear NFC community members,

I am working on designing a small RFID reader circuit that is based on the PN532 chip and I would like to get some feedback. My background isn't RF engineering, so I am not sure about many things.

I'll summarize the main questions first, and then describe in details what I've done:

I am using miniVNA Tiny for taking measurements.

Q1: which parameter (SWR, RP, RL) should I look at for figuring out the self resonance of a circuit?

Sometimes the sign flip of RP correlates well with the minimum of RL and SWR, but not always.

Q2: Why after tuning my antenna to 13.56 Mhz (based on SWR or RL measurements) do I see a huge shift in resonance frequency when I bring a tag close to the antenna? Typically, two peaks appear: one at ~12.8Mhz and one at ~14.3Mhz? Is this normal?

Before:

pastedImage_10.png

After a tag is nearby:

pastedImage_12.png

pastedImage_11.png

Full story below (and more questions below):

I basically followed the reference design and white papers describing how to tune the antenna.

The circuit has the EMC module (560nH, 220pF), series caps (C1) and parallel caps (C2).

At first, I tried to follow the general guidelines which were:

1. Measure antenna inductance (La)

I did this by measuring the reactance at 1Mhz. La = Xs / w0 = 1.6uH

This seems reasonable.

2. Measure antenna self resonance.

I looked either at the sign flip of RP or SWR.

I noticed multiple peaks, which one should I consider to be the resonance?

pastedImage_5.png

3. From the self resonance, estimate the antenna capacitance:

f0=1e6; % measured at 1 Mhz

w0 = 2*pi*f0;

La = Xs/w0;

Fself = 472270937;

Ca = 1/((2*pi*Fself)^2 * La);

4. Calculate C1 and C2.

I followed equations from white paper:

Ra =7.7; % Measured at 1 Mhz

Xs = 9.8; % Measured at 1 Mhz

nfc_freq = 13.56*1e6;

w = 2*pi*nfc_freq;

Qa = w*La/Ra

Rmatch = 30;

Rq = max(0, 0.5 * (w*La / Rmatch - Ra))

% in my case, no series resistors were needed. Q was  ~17

% EMC filter:

L0 = 560 * 10^-9; % 560 nH

Femc_cutoff =14338865.060467; % 14.4 Mhz

C0 =   (1/(Femc_cutoff*2*pi)).^2/Lemc; % 220 pF

% Calculate the series equivalent

Xtr = 2*w * ( L0 * (1-w^2*L0*C0) - Rmatch^2/4 * C0) / ((1-w^2*L0*C0)^2 + (w*Rmatch/2*C0)^2);

Rtr = Rmatch / ( (1-w^2*L0*C0)^2 + (w*Rmatch/2*C0)^2);

% Calculate the parallel equivalent circuit:

Lpa = La;

Cpa = Ca;

Rpa = (w*La)^2 / (Ra + 2*Rq);

C1 = 1/( w* (sqrt(Rtr*Rpa/4) + Xtr/2));

C2 = 1/(w^2 * Lpa/2) - 1/(w * sqrt(Rtr*Rpa/4)) - 2*Cpa;

------

The final result was:

For C1 (26.33), use 4.70 + 22.00 (=26.70), error = 0.370680 pF

For C2 (149.62), use 0.00 + 150.00 (=150.00), error = 0.380073 pF

I tried out these values, but the end result was really out of range.

Did I miss something out in my calculations?

I then played around by changing caps (without the EMC bandpass filter).

I noticed two major trends:

1. When I increase C1, I get a narrower profile (smaller arc on Smith Chart)

2. Increasing C2 generally doesn't change the radius of the arc much, but shifts the resonance frequency downward.

I ended up with this:

pastedImage_8.png

pastedImage_10.png

Does this look reasonable? If so, why do I get such a huge detuning when a tag is near by?

标记 (1)
1 解答
9,117 次查看
shayohayon
Contributor II

OK. I followed the steps laid out in AN1445. That is the most useful document on the issue.

The flow chart for tuning C1 and C2 really helped.

Now the antenna is properly tuned and the circuit works!

A critical step is setting the correct resistance on the receiver voltage divider circuit. I fried my first board because the returned voltage exceeded 1V :smileyhappy:

在原帖中查看解决方案

0 项奖励
回复
4 回复数
9,117 次查看
salmabay
Contributor II

Hello shayohayon,

I will order mini Vna tiny to tune my Antenna, as you mentioned you used it in your design.

Is it working without problems? because NXP recommends to use only mini VNA PRO.

Thank you 

0 项奖励
回复
9,118 次查看
shayohayon
Contributor II

OK. I followed the steps laid out in AN1445. That is the most useful document on the issue.

The flow chart for tuning C1 and C2 really helped.

Now the antenna is properly tuned and the circuit works!

A critical step is setting the correct resistance on the receiver voltage divider circuit. I fried my first board because the returned voltage exceeded 1V :smileyhappy:

0 项奖励
回复
9,117 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Shay,

     I asked for help of NFC expert team on your questions, the following is answers!

----------------------------

Q1: which parameter (SWR, RP, RL) should I look at for figuring out the self resonance of a circuit?

Sometimes the sign flip of RP correlates well with the minimum of RL and SWR, but not always.

[Answer] We just check Rs value for matching when Xs is close to 0 @13.56MHz.

Q2: Why after tuning my antenna to 13.56 Mhz (based on SWR or RL measurements) do I see a huge shift in resonance frequency when I bring a tag close to the antenna? Typically, two peaks appear: one at ~12.8Mhz and one at ~14.3Mhz? Is this normal?

[Answer] It is normal when a tag/card or other metal circuit close to the antenna. The coupling effect will detune the original matching.

More antenna matching guide can be found on the following link:

http://cache.nxp.com/documents/application_note/AN11019.pdf?fpsp=1&WT_TYPE=Application%20Notes&WT_VE...

------------------------------

Regards,

Weidong

0 项奖励
回复
9,117 次查看
shayohayon
Contributor II

Bump? Any takers? Has anyone designed a custom antenna and went through this process before?

0 项奖励
回复