PN5190 Target Current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5190 Target Current

2,704件の閲覧回数
DavidT191624
Contributor I

Dear Sir,

 

We have a NFC reader product would like to use PN5190 chipset. May i know how to setup PN5190 target current without using Nxp cockpit software ? 

According to datasheet , NXP request user to edit EEPROM 0xF9:DPC_Targetcurrent, but i can't found any EEPORM setting is related to this EEPROM address in datasheet. 

May i know how to edit the target current without using cockpit ? 

DavidT191624_0-1690941136732.png

 

Thank you

with regards

David

0 件の賞賛
返信
5 返答(返信)

2,689件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @DavidT191624 

Thanks for contacting us and using the NXP products.

Based on your description, I think what you want to check should be in chapter 9.26 of the datasheet.

NXF92074_0-1690967604255.png

BR

kelly

0 件の賞賛
返信

2,620件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @DavidT191624 

Did you test under DPC mode? or could you share with us how did you test the current?

BR

kelly

0 件の賞賛
返信

2,611件の閲覧回数
DavidT191624
Contributor I

Dear Sir,

 

I measured the current via True RMS multimeter and read the register 0x56 from PN5190 .

 

That's the information i would like to know, how to setup a current limit  with DPC and without DPC. Since my product is not EMV product and the l , this product not suitable use Cockpit calibration method ,

May I know Which register and EEPROM should i adjust ?  and the Procedure ?

 

Thank you

with regards
David

0 件の賞賛
返信

2,590件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @DavidT191624 

It's recommended that you can watch this video, you will be very clear about the DPC feature.

PN5190 Dynamic Power Control Quick Calibration and TxShaping Demo | NXP Semiconductors

BR

kelly

0 件の賞賛
返信

2,656件の閲覧回数
DavidT191624
Contributor I
Dear TechSupport,

I tried to edit this EEPROM but i found that the current does not follow this current limit

Example:

-THe default setting of this EEPROM is 0x0032 (50mA)
-Acutal Current reading via True RMS mulitimeter (200mA)

afte that
I adjust the EEPROM from 50mA to 150mA, but the current meter still got 200mA result and the filed stregth keep same.

May i know how to adjust the target current actually ?
I am using latest firmware V3.0 already
0 件の賞賛
返信