PN5180 Topaz Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5180 Topaz Support

3,170件の閲覧回数
kit_au
Contributor I

Dear Sir, 

We are now developing a contactless reader using PN5180 and completed ISO14443-3A, 4A, 4B and Felica. Now testing on Topaz, I find some problem, please help.

  1. I followed the sample code on "phalT1T.c"
  2. At the beginning, found the timeout too short (or the timer on time not correct) caused the command send problem
  3. increased the timeout value, verified command send no problem, but still cannot receive response
  4. the screenshot below that using smartspy to capture, shown that the card have response to reader (the screenshot shown in unknown characters just because of the antenna position, at least shown card have response)擷取.PNG
  5. The reader register "IRQ_STATUS" return 0x1002 (timeout error)

I cannot find the ways to solve this, please help, thank

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

3,057件の閲覧回数
kit_au
Contributor I

still cannot find the ways to solve

0 件の賞賛
返信

3,057件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

We will continue the support via case.

Regards,

Ivan.

0 件の賞賛
返信

3,057件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

An update was made to the case.

Have a nice day.

Regards,

Ivan.

0 件の賞賛
返信