PN5180 Antenna tuning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN5180 Antenna tuning

3,846 次查看
s04
Contributor I

Hello,

I'm trying to tune the matching circuit of the PN5180.
EMVCo L1 reception test is failing and needs to be resolved.
In the received waveform, the balance between Ich and Qch seems to be unbalanced in the long-distance test.
How can I tune the matching circuit (impedance) to control this IQ balance?
(Currently it matches 20Ω, the RxGain is MAX.)

s04_1-1646708769545.png

s04_0-1646708131602.png

标记 (1)
0 项奖励
回复
2 回复数

3,813 次查看
s04
Contributor I

Thank you !

You mean "Your weakness is not the IQ balance. It may be spike noise."  , right?

0 项奖励
回复

3,823 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello @s04 .

For the application please kindly refer to the document as the attachment.

Hope it help you.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 项奖励
回复