Operational State definition - AN12380

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Operational State definition - AN12380

3,060 次查看
StatBen
Contributor I

In AN12380-2.1.2 (page 5) the capacitance value is specified for the ntag5 ICs. This value is specified with an operational state.

What would be the definition of operational state in this context?

Thanks

 

0 项奖励
回复
6 回复数

3,037 次查看
StatBen
Contributor I

Thanks @KaiLi 

I know about the NFC Antenna tool, but the question here is more about the specific capacitance value according to "operational conditions" here, does operational conditions means the core(digital control unit) is powered or just the rf interface? What were the tests conditions to get that value?

0 项奖励
回复

3,031 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @StatBen ,

according to Table 1 on page 5 of AN12380, specifies the operational state should be the constant voltage, resonance frequency and ambient temperature.

 

Best Regards,

kelly

0 项奖励
回复

3,032 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @StatBen 

There is such a description at the bottom of the fourth page of AN12380, the input capacitance depends on the applied chip voltage. So, specifies the operational state should be the voltage  Vla-lb.

Thanks & Best Regards,

kelly

0 项奖励
回复

3,027 次查看
StatBen
Contributor I

Hi Kelly @KaiLi ,

Thanks, I was wondering in that test case if VCC and Vout were shorted together for energy harvesting and/or if VCC was powered at all.

 

Thanks,
Benoit

0 项奖励
回复

3,019 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @StatBen ,

I think AN12365 might be helpful to you.

thanks for your cooperation 

kind Regards,

kelly 

 

 

 

 

 

0 项奖励
回复

3,043 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @StatBen 

you can use NFC Antenna Tool of NXP to design your application, below is the link:

NFC - NXP Community

For operational state, I understand which is your application conditions, such as the size of the antenna, the contactless distance, etc.

 

Thanks & Best Regards,

kelly

0 项奖励
回复