OM5578/PN7150RPI is compatible with Raspberry Pi Zero W or not?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM5578/PN7150RPI is compatible with Raspberry Pi Zero W or not?

1,476件の閲覧回数
wangqiulin
Contributor I

OM5578/PN7150RPI is compatible with Raspberry Pi Zero W or not? 

If not does any other NFC development board could support Raspberry Pi Zero W?

ラベル(1)
タグ(1)
1 返信

1,395件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

There is no change in the definition of 40 pin GPIO port, so OM5578/PN7150RPI is compatible with Raspberry Pi Zero W.

pastedImage_1.png

pastedImage_2.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------