OM5578/PN7150RPI is compatible with Raspberry Pi Zero W or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM5578/PN7150RPI is compatible with Raspberry Pi Zero W or not?

1,504 Views
wangqiulin
Contributor I

OM5578/PN7150RPI is compatible with Raspberry Pi Zero W or not? 

If not does any other NFC development board could support Raspberry Pi Zero W?

Labels (1)
Tags (1)
1 Reply

1,423 Views
Kan_Li
NXP TechSupport
NXP TechSupport

There is no change in the definition of 40 pin GPIO port, so OM5578/PN7150RPI is compatible with Raspberry Pi Zero W.

pastedImage_1.png

pastedImage_2.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------