OM26630FDK 'correct microcontroller firmware'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM26630FDK 'correct microcontroller firmware'

2,926 Views
lorenzomarcanto
Contributor II

We bought a OM26630FDK kit to test the NFC reader kit; the NFC Cockpit software downloaded and installed properly, also the board is detected correctly (it's seen as COM6). However the log panel says "please use the correct microcontroller firmware for the cockpit version in use". Shouldn't be the kit ready to use? how to make it work?

0 Kudos
Reply
1 Reply

2,357 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please flash the binary (BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin) contained in Cockpit firmware for CLRC663, it is by default in the following path: C:\...\NxpNfcCockpit_v4.7.0.0\firmware\Secondary_RC663

You may flash it by using the MCUXPresso Flash programmer tool. You can take this as reference to know where the tool is:

https://community.nxp.com/thread/449152?commentID=896950#comment-896950

Regards,

Ivan.

0 Kudos
Reply