NXP Tagwriter - Write from CSV

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Tagwriter - Write from CSV

7,666 Views
chrisong_what
Contributor I

Hi Sir/Madam,

 

Good day to you.

 

Kindly check with you the CSV file if i want to add more records in a row, is it possible can do?

 

Thanks.

 

Best Regards, 
Christopher

0 Kudos
Reply
3 Replies

7,365 Views
t_kubicek
Contributor I

Hallo, could you please provide me the correct vcard template how to write multiple contacts eg. up to 200 contacts via NFC NXP TAGWriter into multiple NFC cards.

Please check also my template attached which NXP writer does not accept.

Thanks

Thanks Tomas

 

0 Kudos
Reply

7,539 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Thank you for contacting us. I just checked your case; basically the app allows you to write comma separated values but not more than one record per row, this means that despite you write it either on CSV or "normal" format, you could only add one record per row, please see below for an example of the Comma Separated Value:

pastedImage_2.png

Have a nice day!

BR,

Ivan.

0 Kudos
Reply

4,620 Views
sipos93
Contributor I

Hi @IvanRuiz 

Could I also request a sample of how the CSV content should look like for the application to accept it?
I just want to save plain URL addresses.

For example:
https://1.com
https://2.com
https://3.com

0 Kudos
Reply