NTAG213 Counter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG213 Counter

2,050 Views
AW1511
Contributor I

Hi,

Is there any way to increment the NFC counter on power up? 

The data sheet shows that the counter will not be incremented until a read or fast read command. Is that correct? 

I can think of a number of relevant use cases where counter increment on power up without the need for an external read command would be useful.

Thanks,

Andrew

0 Kudos
Reply
2 Replies

2,007 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well.

The NFC counter will be automatically increased at the first READ or FAST_READ command after a power on reset.

So, the command is necessary to increase the counter value.

 

Best Regards,

Ricardo

0 Kudos
Reply

2,018 Views
AW1511
Contributor I

Is there any update on this counter functionality?

0 Kudos
Reply