NTAG I2CPlus Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG I2CPlus Problem

2,479 Views
manuelbuil
Contributor I

Hi, I´m developing a new board and we want to add to it a NXP NTAG I2CPlus device (NT3H2111) by the moment we only want read the device unique 7 bytes UID using I2C and with an external mobile phone using NFC, we don´t need by the moment communicate between mobile phone and our board, we only want that the mobile phone(using NFC) and the device on our board(using I2C) can read the same 7 bytes UID.

Now I can read with my microcontroller the UID using the I2C, but the NFC interface is not working, I can not read the UID of the Ntag using a mobile phone.

Is it possible from the NFC side to read the Ntag´s UID if we have not configured nothing from the I2c side?

The NT3H2111 is powered from a 3.3V power supply 

I´ve attached a photo of the board with the antenna.

Tags (1)
0 Kudos
Reply
1 Reply

2,390 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

If the UID cannot even be read from the NFC Interface, it is most likely a Hardware problem. It would be helpful to refer to the Antenna Design Guide: https://www.nxp.com/docs/en/application-note/AN11276.zip

Regards,

Ivan.

0 Kudos
Reply