NQ330 CE mode solution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NQ330 CE mode solution

3,210 Views
752303698
Contributor I

Hi,

We want to use NQ330 to achieve payment function. Based on our project, the system is freertos running on  MCU. I noticed there were three interfaces on the NQ330, UART and SPI, SWP. The following list show my concern.

1. If I don't use SWP, how can I use uart and SPI to achieve payment function?

2. For the aim of the security, how can I map the Secure Element? Is it possible to put in inside NQ330? or I need to use SD card which can communicate with NQ330 by SPI?

3. If there are some documents showing the solution and processing flow, demo code about payment function which this NQ330 support. Please help to share it.

Thank you very much for your help and effort, really appreciate it.

BRS

Kelly

0 Kudos
Reply
2 Replies

3,081 Views
752303698
Contributor I

So could please let me know which module is designed for wearable devices. Thank you

0 Kudos
Reply

3,081 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

    NQ330 is designed for mobile / PC application, our team doesn't have authority to support it. We have special team(mobile team) to support it, so if you wants to get more help on it, you can contact local distributor of NXP. Hope it help you.

Have a nice day.

 

 

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply