NHS3100 Android Rejected Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NHS3100 Android Rejected Error

3,994 Views
marinkoruzic
Contributor I

I want to send a configuration to a nhs3100 1724.18 Tag but keep getting "Configuration rejected".

What could cause this error? The Android SW Version is v16...

0 Kudos
Reply
7 Replies

3,765 Views
driesmoors
NXP Employee
NXP Employee

I would advise updating te APP to the latest version. Do you get this error all the time, or only from time to time, when e.g. the connection is not stable?

0 Kudos
Reply

3,765 Views
aresmarser
Contributor III

Hi Sirs,

Is the issue resolved finally?

I also met the problem that the APP TLogger will get an error mesage "Configuration rejected. Retouch the tag and try again" after I clicked the button to send configuration to tag.

My app version is V15.

Thanks,

Arna

0 Kudos
Reply

3,765 Views
driesmoors
NXP Employee
NXP Employee

I don't recognize v1724.18 as an official build from SDK 10, 10.1 or 11. Can you try flashing an image which wa spre-built from the SDK and see if that works?

If still no success, can you provide me with the XML export of NXP's Tag Info Android app?

0 Kudos
Reply

3,765 Views
marinkoruzic
Contributor I

Here is the xml file. 

Where is the file located in the sdk that I need for flashing the firmware?

Thanks for your help. 

0 Kudos
Reply

3,765 Views
driesmoors
NXP Employee
NXP Employee

Hi, Inside the SDK, check sw/nss/app_demo_dp_tlogger/Release. Best,

0 Kudos
Reply

3,765 Views
marinkoruzic
Contributor I

Hi Dries,

thank you for your answer. The new SW Version is now v17 but I get still the same error. "Configuration rejected".

0 Kudos
Reply

3,765 Views
driesmoors
NXP Employee
NXP Employee

You're likely hitting a known SW error in the Android APP that was solved in v17. Can you update the APP via the Google Play Store and try again?

0 Kudos
Reply