NFC reader chipset for iOS VAS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC reader chipset for iOS VAS

3,908件の閲覧回数
jr_hernandez
Contributor II

Hello,

I have been requested to design a NFC reader to be compatible with iOS VAS protocol.

Actually, thge system must be capable of reading NDEF messages from physical Tags, Andoid phone (HCE) and iOS (HCE/VAS). The iOS is the more obscure part since it is not clear if HCE is working as expected.

My plan is to use low power detection and run the ncf poller once it is waken up and read NDEF from whichever device is in front of the antenna.

Which chipset would you recommend me for this application?

Is there any HW or FW require in order to be compliant with iOS VAS?

Regards, Ramon.

 

0 件の賞賛
返信
2 返答(返信)

3,745件の閲覧回数
RobbieF
Contributor I

Hi Ramon - How did you get on with this development?  Have you finished the product as yet?

0 件の賞賛
返信

3,875件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Ramon:

 

Please refer to PN7150X: High-performance NFC controller IC with support for Apple Enhanced Contactless Polling (ECP)

https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/high-performance-nfc-controller-ic-with-sup...

 

To get this and any additional questions related to AVS, please contact your representative at Apple.

 

Regards

Daniel

タグ(1)
0 件の賞賛
返信