NFC - lock / unlock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC - lock / unlock

4,933件の閲覧回数
patrickterreaux
Contributor I

Hi,

I'm new in the NFC world and I'm currently evaluating your NTAG I2C (www.nxp.com/demoboard/OM5569)

As far as I know, it is possible to lock the chip through NFC, so that it is "read only".

My question:

Is it possible through I2C to unlock the chip ?

Thank you in advance

0 件の賞賛
返信
1 返信

4,251件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Patrick Terreaux:

As you mention the NTAG I2C tags have the static lock bytes and dynamic lock bytes to configure different regions of memory to "read-only" mode.

Once the lock bits are set to '1', this is irreversible from RF interface (NFC side), but the bits can indeed be reset to '0' from the I2C interface.

I hope this clarifies.

Have a good day!

Jorge Gonzalez

0 件の賞賛
返信