NFC development kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC development kit

2,108件の閲覧回数
amir_baldari
Contributor I

hello everybody, I have started my master thesis regarding to reading passive sensors with NFC and I am looking for development kits of NXP. kindly, could you help me and suggest the best kit (for example  NHS3152UK could be useful or not )

2 返答(返信)

1,961件の閲覧回数
driesmoors
NXP Employee
NXP Employee

Hi,

I can only comment for the NTAG SmartSensor ICs, i.e. the NHS3100 and the NHS3152.

The UK suffix indicates the package used is the WLCSP25 (2.51x2.51x0.5 mm): pastedImage_1.png

This is not a human-solder-friendly package, to put it mildly.

For a thesis, you're far better off using the HVQFN24 package (4x4x0.85 mm):pastedImage_2.png

These ICs can be bought via distributors or directly from NTAG SmartSensor|NXP 

To support development, we also offer boards and kits with the NHS3100 and NHS3152 ICs.

The NHS3152 offering of kits (PCB containing an NHS3152 HVQFN24 + LPC-Link2 debugger board) is:

The NHS31xx IC can be used both powered and passive. The energy from the RF field is harvested and can be used to power the complete IC (at 1.85V, if I'm not mistaken). In passive mode, all HW blocks and PIOs are functional.

We label the ICs as being semi-passive: a battery is typically used for unattended monitoring, but the energy harvesting feature guarantees full data readout even in case of a battery failure.

Hope this helps somewhat. Good luck with your thesis - whatever your choice.

Kind regards,
Dries.

1,961件の閲覧回数
amir_baldari
Contributor I

dear Dries

many thanks for your helpful feedback

0 件の賞賛
返信