NFC Cockpit not connecting to dev board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Cockpit not connecting to dev board

4,050 Views
robhelvestine
Contributor II

I've installed NFC Cockpit v4.7.0 and plugged in my CLRC663 dev board, but it always says "Disconnected" in the upper left. How do I reinstall the drivers, as I'm assuming that's my problem. Any other tips? Thanks. 

0 Kudos
Reply
5 Replies

3,276 Views
HeMyFAE
NXP Employee
NXP Employee

Dear Rob,

Please see my step by step instruction with in using MCU Xpresso to re flash the 1769 with the Cockpit firmware.

2,425 Views
Anonymous
Deactivated User

Hi, which BIN File should I use, when working with PNEV7462C?

0 Kudos
Reply

3,276 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to the following community thread:

https://community.nxp.com/message/1007043 

If you have any doubt, please let me know.

Regards,

Ivan.

0 Kudos
Reply

3,276 Views
robhelvestine
Contributor II

Hello IvanRuiz‌,

To clarify, I need to download the MCUXpresso IDE, and use that to flash that binary onto the cockpit hardware? Is that correct?

I can't seem to download the MCUXpresso IDE. See the error message below when I click on "download"

pastedImage_1.png

Any help?

0 Kudos
Reply

3,276 Views
robhelvestine
Contributor II

Also IvanRuiz‌,

Here is my log screen when I plug in the Cockpit tool:

pastedImage_1.png

Just want to make sure there is nothing else preventing me from using the tool. Thanks.

0 Kudos
Reply