NFC Cockpit not connecting to dev board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NFC Cockpit not connecting to dev board

4,062 次查看
robhelvestine
Contributor II

I've installed NFC Cockpit v4.7.0 and plugged in my CLRC663 dev board, but it always says "Disconnected" in the upper left. How do I reinstall the drivers, as I'm assuming that's my problem. Any other tips? Thanks. 

0 项奖励
回复
5 回复数

3,288 次查看
HeMyFAE
NXP Employee
NXP Employee

Dear Rob,

Please see my step by step instruction with in using MCU Xpresso to re flash the 1769 with the Cockpit firmware.

2,437 次查看
Anonymous
不适用

Hi, which BIN File should I use, when working with PNEV7462C?

0 项奖励
回复

3,288 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to the following community thread:

https://community.nxp.com/message/1007043 

If you have any doubt, please let me know.

Regards,

Ivan.

0 项奖励
回复

3,288 次查看
robhelvestine
Contributor II

Hello IvanRuiz‌,

To clarify, I need to download the MCUXpresso IDE, and use that to flash that binary onto the cockpit hardware? Is that correct?

I can't seem to download the MCUXpresso IDE. See the error message below when I click on "download"

pastedImage_1.png

Any help?

0 项奖励
回复

3,288 次查看
robhelvestine
Contributor II

Also IvanRuiz‌,

Here is my log screen when I plug in the Cockpit tool:

pastedImage_1.png

Just want to make sure there is nothing else preventing me from using the tool. Thanks.

0 项奖励
回复