NFC Cockpit for Custom Board CLRC663

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NFC Cockpit for Custom Board CLRC663

2,304 次查看
lakshminarayana
Contributor II

Hi, Is there a way where we can use the NFC Cockpit tool for custom boards(has JTAG/USB(Through UART ).

Can we directly use USB(through UART) to access the tool?

If not,

Can we connect the JTAG/UART of the custom board to Eval of CLRC663 LPC Controller and access?

 

Thanks.

0 项奖励
回复
3 回复数

2,276 次查看
lakshminarayana
Contributor II

Any updates on this?

 

0 项奖励
回复

2,292 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

More information please find the application note as the link.

URL:https://www.nxp.com.cn/docs/en/application-note/AN11022.pdf.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复

2,289 次查看
lakshminarayana
Contributor II

I was specifically asking about accessing Cockpit tool with  Custom NFC Front end IC without LPC Controller.

The above document is for EVAL Kit right?

0 项奖励
回复