NFC Cockpit for Custom Board CLRC663

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Cockpit for Custom Board CLRC663

2,331件の閲覧回数
lakshminarayana
Contributor II

Hi, Is there a way where we can use the NFC Cockpit tool for custom boards(has JTAG/USB(Through UART ).

Can we directly use USB(through UART) to access the tool?

If not,

Can we connect the JTAG/UART of the custom board to Eval of CLRC663 LPC Controller and access?

 

Thanks.

0 件の賞賛
返信
3 返答(返信)

2,303件の閲覧回数
lakshminarayana
Contributor II

Any updates on this?

 

0 件の賞賛
返信

2,319件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

More information please find the application note as the link.

URL:https://www.nxp.com.cn/docs/en/application-note/AN11022.pdf.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信

2,316件の閲覧回数
lakshminarayana
Contributor II

I was specifically asking about accessing Cockpit tool with  Custom NFC Front end IC without LPC Controller.

The above document is for EVAL Kit right?

0 件の賞賛
返信