NFC Antenna Tuning using calibration coil

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Antenna Tuning using calibration coil

ソリューションへジャンプ
3,596件の閲覧回数
hengma
Contributor II

Hi,

 

I have a question related to the antenna tuning process of RFID readers using CLRC663. I noticed that all application notes use VNA to measure the impedance at the Tx ports of the chipset. May I know if there is an indirect way to tune the antenna? For example, can we place a calibration coil on the reader and measure the voltage from the calibration coil? A high-impedance probe is used to measure the voltage from the calibration coil. The antenna is tuned using a variable capacitor and is considered to be well-tuned once the maximum voltage from the calibration coil is obtained. May I know if it is feasible?

 

Thanks,

 

Heng

 

 

0 件の賞賛
返信
1 解決策
3,547件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @hengma 

Thanks for contacting us and using the NXP products.

Your approach sounds feasible, but NXP has no such precedent, so it is difficult to give you relevant advice. It is still recommended that you use the method recommended by NXP to achieve it.

BR

kelly

元の投稿で解決策を見る

2 返答(返信)
3,548件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @hengma 

Thanks for contacting us and using the NXP products.

Your approach sounds feasible, but NXP has no such precedent, so it is difficult to give you relevant advice. It is still recommended that you use the method recommended by NXP to achieve it.

BR

kelly

3,478件の閲覧回数
hengma
Contributor II
Thanks for that. Understood.
0 件の賞賛
返信