Multiple lines Vcard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple lines Vcard

6,399件の閲覧回数
MTs
Contributor I

I create a multiple lines nfc tag using the "add more" option and adding a business card + web address.

But I'm not able to create the same tag using the data stored in "My dataset" because using "write multiple" option it doesn't create a multiple lines tag.

And if I use "add more", it's not possible to choose from "my datasets".

Thank you 

0 件の賞賛
返信
5 返答(返信)

6,385件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @MTs 

Could you describe your problem more clearly? For example, which product do you use? Which software is used?

0 件の賞賛
返信

6,380件の閲覧回数
MTs
Contributor I

Thank you for your quick answer!

I use NXP TagWriter on Android phone. I already create a multiple tag, to write it on an NFC tag, that includes both Vcard and internet address, using the "add more" option to create the second line. When I click on "add more" I can just add a new dataset (writing or importing it), but I cannot use a dataset previously stored in "My dataset". This means that I can use "my dataset" just to prepare the first part of the data group (link or Vcard), and not to add the second part.

0 件の賞賛
返信

6,368件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @MTs 

I tested the steps you described and everything works fine. You can't see the previously written message in "My Data", it should be that you did not choose to save the data when you wrote it before. Please try to write and save action.

0 件の賞賛
返信

6,329件の閲覧回数
MTs
Contributor I

Thank you again for your kind answer.

I have multiple set of data in "my dataset" (ScreenShot .......0013) , but when I click on WRITE MULTIPLE and select 2 sets (SS 14), then the content that appear is just one of them (SS ....4950).

And if I click on ADD MORE, it appears the list of NEW DATASETS, in this screen I cannot choose MY DATASET (SS 15).

If I choose MY DATASETs>MORE OPTIONS>WRITE MULTIPLE>ADD MORE>[not from MY DATASETS, but from the list of new datasets that appear]eg:LINK..., in this case aI can create a multiple-line tag (see screenshots n° .....16) 

Thank You

0 件の賞賛
返信

6,312件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @MTs 

Please go to the below link and update Tagwriter, after that your issue will be fixed.

NFC TagWriter by NXP - Apps on Google Play

0 件の賞賛
返信