Multiple lines Vcard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple lines Vcard

6,476 Views
MTs
Contributor I

I create a multiple lines nfc tag using the "add more" option and adding a business card + web address.

But I'm not able to create the same tag using the data stored in "My dataset" because using "write multiple" option it doesn't create a multiple lines tag.

And if I use "add more", it's not possible to choose from "my datasets".

Thank you 

0 Kudos
Reply
5 Replies

6,462 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @MTs 

Could you describe your problem more clearly? For example, which product do you use? Which software is used?

0 Kudos
Reply

6,457 Views
MTs
Contributor I

Thank you for your quick answer!

I use NXP TagWriter on Android phone. I already create a multiple tag, to write it on an NFC tag, that includes both Vcard and internet address, using the "add more" option to create the second line. When I click on "add more" I can just add a new dataset (writing or importing it), but I cannot use a dataset previously stored in "My dataset". This means that I can use "my dataset" just to prepare the first part of the data group (link or Vcard), and not to add the second part.

0 Kudos
Reply

6,445 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @MTs 

I tested the steps you described and everything works fine. You can't see the previously written message in "My Data", it should be that you did not choose to save the data when you wrote it before. Please try to write and save action.

0 Kudos
Reply

6,406 Views
MTs
Contributor I

Thank you again for your kind answer.

I have multiple set of data in "my dataset" (ScreenShot .......0013) , but when I click on WRITE MULTIPLE and select 2 sets (SS 14), then the content that appear is just one of them (SS ....4950).

And if I click on ADD MORE, it appears the list of NEW DATASETS, in this screen I cannot choose MY DATASET (SS 15).

If I choose MY DATASETs>MORE OPTIONS>WRITE MULTIPLE>ADD MORE>[not from MY DATASETS, but from the list of new datasets that appear]eg:LINK..., in this case aI can create a multiple-line tag (see screenshots n° .....16) 

Thank You

0 Kudos
Reply

6,389 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @MTs 

Please go to the below link and update Tagwriter, after that your issue will be fixed.

NFC TagWriter by NXP - Apps on Google Play

0 Kudos
Reply