MIFARE reader malfunctioning during EMC tests

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIFARE reader malfunctioning during EMC tests

2,098件の閲覧回数
nicolamagistrel
Contributor I

Hello everybody,

I am facing an issue with the Mifare reader MFRC63002, when it is exposed to conducted disturbances by electromagnetic fields by using an absorbing clamp:

by setting the amplitude of the disturbance equal to 1V (AM 1KHz), when the frequency of the disturbance becomes a multiple of the quartz crystal frequency 27.12MHz the MFRC63002 chip stops working properly (the chip is not able to detect anymore the presence of a valid MIFARE classic or plus tag).

By analyzing the issue, we could see that when the problem occurs the following bits of the error register (addr. 0x0A), analyzed during the receiving phase, are set:

bit 4 MinFrameErr

bit 2 CollDet

The configuration registers of the transmitter and receiver are programmed with their default factory values.

Then, we modified the RxAna register (addr, 0x39) in order to reduce the Rx Gain and the RxThreshold register (addr. 0x37) in order to increase the MinLevel, but we did not get meaningful improvements.

Has anybody faced a similar problem like the one described above ? If yes, which countermeasures have been taken to solve or at least mitigate the issue?

Thanks in advance for your support.

Best regards,

Nicola Magistrelli.

0 件の賞賛
返信
2 返答(返信)

1,970件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Nicola,

This issue is related with the electromagnetic shielding, changing the register configuration would not help much. We provide a training video on that topic, please refer to NFC Antenna Design 6: EMC related Design|NXP  for details.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,970件の閲覧回数
nicolamagistrel
Contributor I

Hi Kan,

Thanks a lot for your comment.

Have a nice day,

Nicola

Da: Kan_Li

Inviato: venerdì 21 settembre 2018 10:52

A: Magistrelli Nicola <[email protected]>

Oggetto: Re: - Re: MIFARE reader malfunctioning during EMC tests

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: MIFARE reader malfunctioning during EMC tests

reply from Kan_Li<https://community.nxp.com/people/Kan_Li?et=watches.email.thread> in NFC - View the full discussion<https://community.nxp.com/message/1060135?commentID=1060135&et=watches.email.thread#comment-1060135>

0 件の賞賛
返信