MFRC63002 & CLRC66303HN NfcrdlibEx1_BasicDiscoveryLoop porting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFRC63002 & CLRC66303HN NfcrdlibEx1_BasicDiscoveryLoop porting

2,261件の閲覧回数
join_ren
Contributor III

Hello

I‘m porting NfcrdlibEx1_BasicDiscoveryLoop in CLEV6630B+RT1052 . It can read Type A card.

If I replace development board CLRC66303HN to MFRC63002. 

I check datasheet CLRC66303HN & MFRC63002 is Pin to Pin. 

Question: Does the HW & SW need to be modified ? 

ラベル(2)
4 返答(返信)

2,153件の閲覧回数
join_ren
Contributor III

Hello

Thanks for your support.  This problem has been resolved.

 

2,153件の閲覧回数
join_ren
Contributor III

Hello,

In AN11256 document description “ To setup the main protocol settings for MFRC631, MFRC630 or SLRC610 the “loadprotocol” must be used. ”

How to 'loadprotocol' .  If I use MFRC630.

Thanks.

0 件の賞賛
返信

2,153件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

But there is also the mention there that for MFRC631 and MFRC630 the supported protocol numbers stay the same. So for both derivates the “PHHAL_HW_RC663_RXTX_xxx” table, in the phhalHw_Rc663_Int.h file doesn’t need to be changed.

Still, in the SDK you can check the phhalHw_Rc663_Cmd_LoadProtocol .

Regards,

Estephania

0 件の賞賛
返信

2,153件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

you will need to perform some modifications, still, I believe that you can find them in the application note AN11256, could you please check it and verify if this is what you were looking for?

 

Regards
Estephania

0 件の賞賛
返信