MFRC63002 & CLRC66303HN NfcrdlibEx1_BasicDiscoveryLoop porting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFRC63002 & CLRC66303HN NfcrdlibEx1_BasicDiscoveryLoop porting

2,244 Views
join_ren
Contributor III

Hello

I‘m porting NfcrdlibEx1_BasicDiscoveryLoop in CLEV6630B+RT1052 . It can read Type A card.

If I replace development board CLRC66303HN to MFRC63002. 

I check datasheet CLRC66303HN & MFRC63002 is Pin to Pin. 

Question: Does the HW & SW need to be modified ? 

Labels (2)
4 Replies

2,136 Views
join_ren
Contributor III

Hello

Thanks for your support.  This problem has been resolved.

 

2,136 Views
join_ren
Contributor III

Hello,

In AN11256 document description “ To setup the main protocol settings for MFRC631, MFRC630 or SLRC610 the “loadprotocol” must be used. ”

How to 'loadprotocol' .  If I use MFRC630.

Thanks.

0 Kudos
Reply

2,136 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

But there is also the mention there that for MFRC631 and MFRC630 the supported protocol numbers stay the same. So for both derivates the “PHHAL_HW_RC663_RXTX_xxx” table, in the phhalHw_Rc663_Int.h file doesn’t need to be changed.

Still, in the SDK you can check the phhalHw_Rc663_Cmd_LoadProtocol .

Regards,

Estephania

0 Kudos
Reply

2,136 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

you will need to perform some modifications, still, I believe that you can find them in the application note AN11256, could you please check it and verify if this is what you were looking for?

 

Regards
Estephania

0 Kudos
Reply