MFRC630 no response ATQA to request ALL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFRC630 no response ATQA to request ALL

2,281 Views
gksrb4
Contributor I

hi i  have developed the card reader device using mfrc630plus,

Our device can read and write mifare classic card.

but desfire, jcob card doesn't response about request ALL.

I not sure that this issue is about h/w (tuning) or f/w (register setting) etc...

h/w developer is said that the antenna tuning is not perfect but well. 

I will wait to your advice.

0 Kudos
Reply
2 Replies

2,031 Views
santosh2
Contributor I

Hello All,

I am also using MFRC630plus reader chip with MSP430 Microcontroller,

As i understand you were able to read the Mifare classic card using the reader chip,

I would request if possible can you please help me as i am stuck up with this,

Please share if any reference or bare minimal code if possible which i can refer and test the basic reading functionality with mifare classic card

Thanks and Regards

Santosh P

 

0 Kudos
Reply

2,188 Views
Kan_Li
NXP TechSupport
NXP TechSupport

We provide sample projects for desfire in the NFC reader library, and you may request from the docstore.

pastedImage_1.png

Please refer to the attachment for more details.

Hope that helps,


Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply