Linux Driver for PN7462?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux Driver for PN7462?

2,312 Views
johnkcfu
Contributor I

I'm planing to use PN7462 to access a Mifare card reader and a Mifare SAM card reader for 2 SAM cards via USB CCID protocol. Besides, we have to provide the solution under Linux development.

The question is that is it possible to use PN7462 using a driver for LINUX? Since from the datasheet I could see Windows deriver supported only.

Thanks.

0 Kudos
Reply
1 Reply

1,867 Views
ND2
Contributor III

@john Fu

We also face the same challenge and have already reviewed the NXP community page link:

https://community.nxp.com/docs/DOC-334952 

But there is no progress on our end.

Since this post is a year old now, I was wondering if you ever reached the solution.

Neel.

0 Kudos
Reply