Is it possible to copy the signature and READ_SIG command of NTAG21x?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to copy the signature and READ_SIG command of NTAG21x?

2,031 Views
naotoikeda
Contributor I

Is it possible to copy the signature and READ_SIG command of NTAG21x?

There is the signature function on NTAG21x for a brand protection.

However I think if other malign IC maker copy the NTAG21x including the signature and READ_SIG, we cannot judge if the IC is made by NXP or not.

I think we can verify it if the signature is  generated by UID and private key.

Best Regards,

Naoto.

Labels (1)
0 Kudos
Reply
1 Reply

1,566 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Naoto Ikeda, Hope you are doing great, Each NTAG supporting the originality signature holds a 32-byte cryptographic signature based on elliptic curve cryptography. This signature can be retrieved using a dedicated
command and can be verified using the corresponding ECC public key in the NFC
device. please check the AN11350 NTAG Originality Signature Validation here is the explanation about this procedure hopefully it will answer your question.

BR

Jonathan

0 Kudos
Reply