I2C timeout when using NT3H2111

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C timeout when using NT3H2111

1,668 Views
hrj
Contributor I

Hello.

 

I've implemented bidirectional communication using SRAM as described in AN11579 using the NT3H2111 chip.

 

This works as a charm most of the times, but occasionally a command sent via I2C times out, and then the chip becomes unresponsive, and all subsequent commands times out.

 

I’ve tried to perform the soft reset as described in 9.3 p 42 in the manual, but that does not solve the issue.

 

What can I do except resetting the whole device?

 

Regards

Henrik Rune Jakobsen

Tags (1)
0 Kudos
Reply
1 Reply

1,600 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Henrik Rune Jakobsen,

Would you please download the MCUXpresso SDK with NTAG I2C software component added?

NTAG I2C Add software component.png

Then you will find the ntag_i2c_explorer_demo in it's folder.(for example: ...\SDK_2.3.1_FRDM-KL02Z\boards\frdmkl02z\demo_apps\ntag_i2c_plus\ntag_i2c_explorer_demo)
It will show you how to use pass-through mode.

ntag_i2c_explorer_demo.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply