How to generate Hardware interrupt to wake MCU from deep power down when the card is detected?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to generate Hardware interrupt to wake MCU from deep power down when the card is detected?

Jump to solution
2,628 Views
mahendrasondaga
Contributor III

Hello freaks,

I'm dealing with the battery  operated NFC based application and i need to conserve the battery as much as i can.

For the card R/W and P2P mode I'm using PN7150. I know about it's Low power card detection mode (LPCD) to significantly reduced power consumption but i also need to put my Host processor in Deep power down and need to wake-up when the card enters in filed (just like NT3H1101 FD pin and PN532 P70_IRQ)  can any one guide me here

Thanks

0 Kudos
Reply
1 Solution
2,265 Views
IvanRuiz
NXP Employee
NXP Employee
0 Kudos
Reply
2 Replies
2,266 Views
IvanRuiz
NXP Employee
NXP Employee
0 Kudos
Reply
2,265 Views
mahendrasondaga
Contributor III

Hello there ..
I'm eagerly waiting for the support from nxp community...
can any one help me here

0 Kudos
Reply