How to export PN7462 projects from MCUXpresso IDE with linked resources

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to export PN7462 projects from MCUXpresso IDE with linked resources

1,276件の閲覧回数
gkowshik
Contributor II

Hi, 

I am having a project that has multiple libs like USB and NFC libs etc., However I want a neat & efficient way to export this project as a zip file so that the project runs straight on other's PC without re-configuring the include paths and libs path etc., 

How can we keep the linked resources while exporting? The method of using "Export -> Archive File -> ticked the resolve and export linked resources" did not work. 

Please help me resolve this as other colleagues need to use this project and compile on their side.

Thanks,
G Kowshik

0 件の賞賛
返信
3 返答(返信)

1,249件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

I would suggest you zip your reader library

 

Regards Daniel

0 件の賞賛
返信

1,244件の閲覧回数
gkowshik
Contributor II

I guess my question wasn't clear. The libs are coming from the SDK that is provided by NXP. We are simply making a link to it in the software by providing the paths. I don't see a reason why I should zip my library and also I am not able to zip it from the Export window from the IDE.

Thanks

0 件の賞賛
返信

1,227件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

 

Please refer to MCUXpreso IDE User Guider,  Chapter 9.4  Exporting Projects

This doc is under the MCUXpresso IDE installation folder

 

Regards

Daniel

0 件の賞賛
返信