How to export PN7462 projects from MCUXpresso IDE with linked resources

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to export PN7462 projects from MCUXpresso IDE with linked resources

1,271 Views
gkowshik
Contributor II

Hi, 

I am having a project that has multiple libs like USB and NFC libs etc., However I want a neat & efficient way to export this project as a zip file so that the project runs straight on other's PC without re-configuring the include paths and libs path etc., 

How can we keep the linked resources while exporting? The method of using "Export -> Archive File -> ticked the resolve and export linked resources" did not work. 

Please help me resolve this as other colleagues need to use this project and compile on their side.

Thanks,
G Kowshik

0 Kudos
Reply
3 Replies

1,244 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

I would suggest you zip your reader library

 

Regards Daniel

0 Kudos
Reply

1,239 Views
gkowshik
Contributor II

I guess my question wasn't clear. The libs are coming from the SDK that is provided by NXP. We are simply making a link to it in the software by providing the paths. I don't see a reason why I should zip my library and also I am not able to zip it from the Export window from the IDE.

Thanks

0 Kudos
Reply

1,222 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

 

Please refer to MCUXpreso IDE User Guider,  Chapter 9.4  Exporting Projects

This doc is under the MCUXpresso IDE installation folder

 

Regards

Daniel

0 Kudos
Reply