How do you put the MFRC630 in I2C fast mode+?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do you put the MFRC630 in I2C fast mode+?

1,049 Views
robhelvestine
Contributor II

How do you put the MFRC630 in I2C fast mode+? It says it is supported, but doesn't describe how to enter this mode, instead of regular I2C speed. 

Thanks,

Rob

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

970 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Rob,

The device supports this mode in hardware, so no additional setup needed to enter this mode. Please refer to Fast Mode Plus - I2C Bus  for more details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply