NHS3100 RTC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NHS3100 RTC

1,675 Views
fantasy
NXP Employee
NXP Employee

My customer used NHS3100 internal RTC with 32kHz FRO clock. There's considerable deviation for the RTC.

At room temperature, the deviation is less than 10s per two days;

If placed two boards in the fridge, where the ambient temp is about -10~-20℃, the deviation between the two boards is about 20min per day. While with sw calibration, the deviation could be reduced to several minutes. 

Customer questions are:

1. Do we have the accuracy characteristic of the internal 32kHz FRO clock/ RTC?

2. Do we have ANs or suggestions to improve the RTC accuracy of wide circumstance temp range?

Labels (1)
0 Kudos
Reply
1 Reply

1,559 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Fantasy,

If you download the NHS3100 SDK(https://www.nxp.com/webapp/Download?colCode=RELEASE-MRA2-NHS3100-11_2&appType=license&Parent_nodeId=... ), you may find the app note on this topic in that package. Please refer to the following for more details.

pastedImage_247.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply