FOR testmod in CLRC663 to measure analog signal.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FOR testmod in CLRC663 to measure analog signal.

1,065 Views
waynejeong
Contributor II

Hello

We have a problem to get EVMco in type B test. So we want to measure analog signal through AUX1, AUX2.

We can see how to enter testmod and what we can set analog signal which we want to measure with application note(AN11019). 

pastedImage_1.png

But I am not sure when I must to call the command. Do I have to execute before send request B or type B setting?

If you have a example source code please let me get it. If not, please explain for me the process details. 

Thank you

0 Kudos
Reply
2 Replies

977 Views
waynejeong
Contributor II

Hello

I have solved this issue using NFC cockpit.

Thank you.

0 Kudos
Reply

977 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

It is good that you were able to solve it.

You can also check this EMVCo L1 Contactless certification process  maybe it can help through your process.

Regards,
Estephania

0 Kudos
Reply