FOR testmod in CLRC663 to measure analog signal.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FOR testmod in CLRC663 to measure analog signal.

1,055件の閲覧回数
waynejeong
Contributor II

Hello

We have a problem to get EVMco in type B test. So we want to measure analog signal through AUX1, AUX2.

We can see how to enter testmod and what we can set analog signal which we want to measure with application note(AN11019). 

pastedImage_1.png

But I am not sure when I must to call the command. Do I have to execute before send request B or type B setting?

If you have a example source code please let me get it. If not, please explain for me the process details. 

Thank you

0 件の賞賛
返信
2 返答(返信)

967件の閲覧回数
waynejeong
Contributor II

Hello

I have solved this issue using NFC cockpit.

Thank you.

0 件の賞賛
返信

967件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

It is good that you were able to solve it.

You can also check this EMVCo L1 Contactless certification process  maybe it can help through your process.

Regards,
Estephania

0 件の賞賛
返信