Example10-MIFARE DESFIRE not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example10-MIFARE DESFIRE not found

4,030 Views
jonnyrabovsky
Contributor I

Hi,

i am testing the PN5180 eval Board,

But there is no Example 10 – MIFARE DESFIRE in the S3522.zip as described in UM10954 PN5180 SW Quick start guide.  

Please tell me where to find it....

Jonny

Labels (1)
0 Kudos
Reply
6 Replies

3,534 Views
steven_kedward
Contributor I

I am also looking for this. Was this solved?

0 Kudos
Reply

3,534 Views
trong-nghiachen
Contributor I

I'm also searching for this sample project " Example 10 – MIFARE DESFire".
Where is the project?

0 Kudos
Reply

3,534 Views
theoz
Contributor II

Hi,

someone can tell me which file in the Docstore i must download for  EXAMPLE 10 MIFARE DESFire?

Thanks

0 Kudos
Reply

3,534 Views
jonnyrabovsky
Contributor I

Hi,

i downloaded the following files(packed into the PDF) via NXP-Docstore:

sw352213 SW3522-NFC-Reader-Library-V40300300001627-R1-for-PNEV5180B-including-all-software-examples.zip

maybe i'm blind, but even there is NO Example10

any suggestions ?

0 Kudos
Reply

3,534 Views
clavin1a
Contributor I

I have the same problem... I have tried to register in NXP DocStore  but I can't... the registration process never end...

If someone has it, please attach it... 

Thanks.

0 Kudos
Reply

3,534 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jonny / Carlos,

The EXAMPLE 10 for MIFARE DESFire is only available in the DocStore portal as mentioned in the Quick Start Guide.

pastedImage_2.png

To access this package in the portal you need to sign a NDA. Please contact your NXP sales representative if you have one already or refer to your local distributor from the next link:

Distributor Network|NXP 


Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply