Encryption options using CLRC663

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Encryption options using CLRC663

1,909 次查看
ghighland
Contributor I

We're using a CLRC663 and MiFARE Ultralight C cards with v4.040.05.011646 of the NXP Reader Library.

We're researching what options are available to us with the NXP Reader Library to encrypt/decrypt the data we're writing to the cards so it cannot be copied/forged.

The documentation that comes with the NXP Reader Library documents the phalMful_UlcAuthenticate() API, but I'm unsure what needs to be configured, both on the reader side and on the application that data-fills the cards, in order to use authentication.

Are there examples available to show how MiFARE Ultralight C cards can be used securely with the NXP Reader Library?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,702 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

I believe that the CLEV6630B NFC Reader Library Including all software examples (Sw297845) would be helpful for you.

Nonetheless, this information is under NDA (Non-Disclosure Agreement) for which you will be asked to register in Docstore. 

Also, as this is under NDA if you have questions regarding the topic you will need to submit the question through a case in the Support|NXP. 

Best Regards, 

Estephania 

0 项奖励
回复