PN7462 Eval GPIO use and running without debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 Eval GPIO use and running without debugger

1,694件の閲覧回数
turbo2ltr
Contributor I

I'm trying to trigger GPIO outputs with a card read. Seems simple enough, but only some of the outputs are working, Other outputs put out a very short pulse when the bit is set on. 

Looking at the full board schematic (which for some reason is not included in the kit) it seems some GPIO pins are shared with the debugger. GPIO 5,6,7,8.  Am I correct in that if you are using the debugger, you cannot use these pins as GPIO?  

If I wanted to run the eval board stand alone, how would I do that?  If I boot it without the debugger connected, nothing happens.

I will need the HSU next. Are those pins also used with the debugger? Or will I be able to use them while the debugger is connected?

0 件の賞賛
返信
1 返信

1,487件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Mike,

(1) Configure them to be GPIO: No problem.

See UM10858.pdf : https://www.nxp.com/docs/en/user-guide/UM10858.pdf

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

(2) Debugger will use SWD interface.

Have a nice day!

TIC weidong sun

0 件の賞賛
返信