Driving the CLRC663 using K60-based MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Driving the CLRC663 using K60-based MCU

2,135件の閲覧回数
MWMinor
Contributor V

I want to drive the CLRC663 with our custom K60-based board. The custom board is similar in architecture to the TWR-K60 board.

Using the application note NFC Reader Library Porting FRDM_K64F, I have successfully built a version of the basic discovery loop project, which compiles and downloads to the target.

When the program runs, I can see the SPI bus is communicating with the CLRC663, and the message "BasicDiscoveryLoop Example: " prints on the console. But the board doesn't respond to the EV3 card.

The program appears to be stuck in a loop within phOsal_NullOs.c...

MWMinor_1-1719406945951.png

It seems the condition is never met to set Status = PH_OSAL_SUCCESS;

The main differences between the FRDM64F set-up and the custom boards is the use of SPI1 for the communication through PORTB. I have attached the header file I created to this post to hopefully assist.

Hope someone can help here....

MWM

 

 

0 件の賞賛
返信
1 返信

2,117件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @MWMinor

We will continue the communication in your internal ticket.

Have a nice day!

Regards,
Eduardo.

0 件の賞賛
返信