Driving the CLRC663 using K60-based MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driving the CLRC663 using K60-based MCU

2,118 Views
MWMinor
Contributor V

I want to drive the CLRC663 with our custom K60-based board. The custom board is similar in architecture to the TWR-K60 board.

Using the application note NFC Reader Library Porting FRDM_K64F, I have successfully built a version of the basic discovery loop project, which compiles and downloads to the target.

When the program runs, I can see the SPI bus is communicating with the CLRC663, and the message "BasicDiscoveryLoop Example: " prints on the console. But the board doesn't respond to the EV3 card.

The program appears to be stuck in a loop within phOsal_NullOs.c...

MWMinor_1-1719406945951.pngMWMinor_1-1719406945951.png

It seems the condition is never met to set Status = PH_OSAL_SUCCESS;

The main differences between the FRDM64F set-up and the custom boards is the use of SPI1 for the communication through PORTB. I have attached the header file I created to this post to hopefully assist.

Hope someone can help here....

MWM

 

 

0 Kudos
Reply
1 Reply

2,100 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @MWMinor

We will continue the communication in your internal ticket.

Have a nice day!

Regards,
Eduardo.

0 Kudos
Reply